SANTA CLARA, Calif., March 31, 2014
Agilent Technologies Inc. (NYSE: A) today announced the successful validation of its T3111S NFC Test System for NFC Forum Analog testing.
During its members' meeting March 17-21 in San Francisco, the NFC Forum confirmed that the Agilent T3111S is one of the first test tools approved for NFC Forum Analog testing. The validation house selected by the NFC Forum performed extensive testing, including comparisons using other candidates' tools.
The T3111S was validated for NFC Forum Digital Protocol testing in 2011. With today's announcement, test laboratories are now equipped to use the T3111S to expand their NFC Forum conformance test programs to include Analog testing. The Analog compliance-assured package is a suite of 33 additional tests comprised of 11 poll-mode and 22 listen-mode cases. The solution is complemented by the Agilent T1142A Automatic Positioning Robot to ensure maximum positioning accuracy and repeatability.
"We are delighted to have received this recognition from the NFC Forum," said Joe DePond, vice president and general manager of Agilent's Mobile Broadband Operation. "We are committed to working with the NFC Forum and our customers worldwide to support the smooth mass adoption of NFC technology."
"It is great to have the Agilent T3111S aligned with the present testing requirements in the market," said Paula Hunter, NFC Forum executive director. "We are pleased to see Agilent's continued investment in NFC certification testing and expect their expertise to make a difference in the success of this technology."
In addition to the validated NFC Forum Digital Protocol and Analog testing capability, the T3111S also supports testing for NFC Forum peer-to-peer protocols, LLCP and SNEP, with validation currently under way.
The Agilent T3111S NFC test system is used worldwide by silicon, reference-design mobile-phone, card and terminal developers; testing laboratories; and operators. The integrated and easy-to-use Agilent system has been widely adopted and supports popular NFC, contactless, ISO and RFID test methodologies.
Agilent Technologies Inc. (NYSE: A) is the world's premier measurement company and a technology leader in chemical analysis, life sciences, diagnostics, electronics and communications. The company's 20,600 employees serve customers in more than 100 countries. Agilent had revenues of $6.8 billion in fiscal 2013. Information about Agilent is available at www.agilent.com.
On Sept. 19, 2013, Agilent announced plans to separate into two publicly traded companies through a tax-free spinoff of its electronic measurement business. The new company is named Keysight Technologies, Inc. The separation is expected to be completed in early November 2014.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@agilent.com
Twitter: @JSmithAgilent
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@agilent.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@agilent.com