SANTA ROSA, Calif., Jan. 6, 2015
Keysight Technologies, Inc. (NYSE: KEYS) today introduced the industry's most complete compliance test application for systems using low-power double-data-rate 4 memory. The application gives engineers an efficient and quick way to characterize LPDDR4 designs.
In addition to testing and validating designs to ensure compliance with the LPDDR4 JEDEC JESD209-1 standard, the application offers offline testing support for running signals from simulation tools like Keysight's Advanced Design System. From simulation to debug and compliance, Keysight is the only test and measurement company that offers hardware and software solutions across all stages of DDR chip development.
The Keysight N6462A DDR4 and LPDDR4 test application, which runs on Keysight Infiniium 90000A, 90000 X-Series and Z-Series oscilloscopes, provides LPDDR4 physical-layer compliance measurements. Signal access is provided by Keysight's LPDDR4 BGA probes.
LPDDR4 is a type of dynamic random-access memory technology optimized for embedded and mobile applications. With its low power requirements, the technology is ideal for mobile devices such as smart phones. LPDDR4 DRAM, with data rates up to 4266 MT/s, is 50 percent faster than current LPDDR3 DRAM.
The Keysight LPDDR4 compliance test application is designed for engineers who develop smart phones, tablets, gaming consoles and other consumer electronics. The N6462A provides automated testing capabilities for clock, electrical, timing and eye diagram tests. The N6462A LPDDR4 application automatically configures the oscilloscope for each test and generates an HTML report at the end of the test. The report compares the results with the specified test limit and indicates how closely the device passes or fails each test.
To complement its LPDDR4 solutions, Keysight offers LPDDR4 BGA probing solutions to provide the LPDDR4 signal accessibility needed to perform physical-layer characterization, protocol analysis and compliance tests. The N6462A LPDDR4 compliance test integrates InfiniiSim and PrecisionProbe tools to enable de-embedding, which removes probing effects, thereby improving measurement accuracy.
"By automating setup with the compliance test software, engineers can save significant test time and ensure their LPDDR4 systems are compliant," said Dave Cipriani, vice president and general manager of Keysight's Oscilloscope and Protocol Division. "The new LPDDR4 compliance test application completes Keysight's LPDDR4 solution portfolio, from simulation to physical-layer and protocol testing."
U.S. Pricing and Availability
The Keysight N6462A DDR4 and LPDDR4 compliance test application is available now for $4,500. An upgrade from the current N6462A DDR4 compliance software test application to include support for LPDDR4 is available with N6462A-2FP, priced at $2,000. Contact Keysight at www.keysight.com/find/contactus for BGA probe pricing and availability.
Additional information
Additional information about Keysight's LPDDR4 compliance test solution is available at www.keysight.com/find/n6462a. Product images are available at www.keysight.com/find/n6462a_images.Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com