Highlights:
- Test and log data over a longer period of time with extended battery life
- Protect against dust and immersion of water with IP 67 certification
- Perform data logging and analysis with the Handheld Meter Logger software
SANTA ROSA, Calif., Nov. 10, 2015
Keysight Technologies, Inc. (NYSE: KEYS) today announced two new series of handheld digital multimeters (DMMs). In addition to offering the capabilities and measurement functions needed for the electronics and industrial test segments, the U1280 Series and U1240C Series handheld DMMs are extremely rugged and come with extended battery life to allow users to test and log data over a longer period of time.
With 60,000-count display resolution and 0.025 percent accuracy, the U1280 Series is Keysight's highest performance handheld DMMs. These 4.5-digit handheld DMMs offer the precision, accuracy and repeatability engineers need to meet the toughest requirements for electronics manufacturing, installation and maintenance work in the electronics test industry.
The U1240C Series 4-digit handheld DMMs come with 10,000-count display resolution and 0.09 percent accuracy, and provide a broad range of measurement functions for installation and maintenance work in industrial facilities. The U1240C Series also comes with unique features such as ZLOW and harmonic ratio. ZLOW provides low impedance mode to eliminate stray voltages. The harmonic ratio function gives an indication of the presence of harmonics.
"With extended battery life and IP 67 certification, the U1280 Series and U1240C Series are designed to be reliable, durable and robust," said Ee Huei Sin, vice president, Keysight's General-Purpose Electronic Measurement Division. "With these new handheld DMMs, engineers can confidently perform tests and troubleshoot over a longer period of time even in tough electronics or industrial settings."
The U1280 Series and U1240C Series are very robust and are suited for operation in the field. These handheld DMMs are certified to IP 67 for complete protection against dust and immersion of water up to one meter, and are capable of withstanding up to a three-meter (ten feet) drop. Additionally, the U1240C Series is CAT IV 600 V and CAT III 1000 V compliant to improve user safety in electrical testing and measurement. Both series of handheld DMMs come with extended battery life – 800 hours for the U1280 Series and 400 hours for the U1240C Series – so users can continue testing for longer periods of time. This is especially important for industrial test engineers whose ultimate goal is to keep the production line running seamlessly to prevent unplanned shutdowns.
For advanced functions and data logging capabilities, engineers can use the Handheld Meter Logger software, which is available at www.keysight.com/find/hhmeterlogger. This PC software allows users to automatically log data in a trend plot or table format, or to manually log each measurement with a touch of a button. Subsequently, users can convert the logged data into various test report formats. For remote monitoring, the U1280 Series and U1240C Series are compatible with the Keysight remote link solution, enabling safer and more convenient testing in hazardous environments.
U.S. Pricing and Additional Information
The new U1280 Series 4.5-digit handheld DMMs and U1240C Series 4-digit handheld DMMs are available worldwide, at the following prices:
Product |
Model |
Description |
Price |
U1280 Series |
U1281A |
True RMS 60,000-count handheld digital multimeter |
$450 |
U1282A |
True RMS 60,000-count handheld digital multimeter |
$500 |
|
U1240C Series |
U1241C |
True RMS 10,000-count handheld digital multimeter |
$280 |
U1242C |
True RMS 10,000-count handheld digital multimeter |
$300 |
Additional information about the U1280 Series 4.5-digit handheld DMMs is available at www.keysight.com/find/U1282A_pr. Information about the U1240C Series 4-digit handheld DMMs is available at www.keysight.com/find/U1242C_pr. High-resolution images are available at www.keysight.com/find/handhelddmms_images. A product video is available at www.keysight.com/find/handhelddmms_video. A complete list of handheld tools videos is available at Keysight's Handheld Tools YouTube channel.
Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com