Keysight Technologies to Demonstrate Electro-Thermal Solver at IMS 2015

  
  

Solution Helps Component Designers Accurately Simulate Temperature Effects in RFIC/MMIC Circuits

SANTA ROSA, Calif., May 13, 2015

Keysight Technologies, Inc. (NYSE: KEYS) today announced it will demonstrate the Advanced Design System (ADS) Electro-Thermal Simulator at the IEEE MTT-S International Microwave Symposium (IMS) 2015, Booth 739, Phoenix, May 17-22. The solution provides accurate, temperature aware IC simulation results by using device temperatures that take into account thermal coupling and thermal characteristics of the RFIC/MMIC component packaging.

IMS is the premier annual international meeting for technologists involved in all aspects of microwave theory and practice. It consists of a full week of events, including paper presentations, tutorials and workshops, as well as an exhibition featuring more than 550 companies.

Keysight experts will demonstrate critical capabilities of the Electro-Thermal Simulator, including:

  • Accuracy, realized in the solution's temperature-aware circuit simulation results based on state-of-the-art thermal solver technology
  • Efficiency, brought about through the solution's direct integration with the ADS layout environment and circuit simulators, which eliminates the need to transfer data to stand-alone thermal solvers
  • Speed, stemming from the solution's high capacity thermal solver technology, which has been tested on SoC designs with thousands of components

The ADS Electro-Thermal Simulator supports 1) steady-state (harmonic balance, DC, AC, S-parameter) analysis, and 2) transient and envelope analyses. Engineers can use the simulator with GaAs, Si and SiGe, as well as a number of other process technologies.

The simulator runs on the Linux 64-bit OS platform and also will soon support the Microsoft Windows OS platform.

A webcast highlighting the functionality of the Electro-Thermal Simulator will take place on June 4. The webcast, "Avoid Design Hazards and Improve Performance with Electro-Thermal Simulation," will explore the use of full electro-thermal analysis to provide accurate electrical and thermal results with full chip capacity and submicron resolution.

Additional information about IMS 2015 is available at www.ims2015.org. An image of the ADS Electro-Thermal Simulator is available at www.keysight.com/find/Electro-ThermalSimulator_images.

About Keysight EEsof EDA Software

Keysight EEsof EDA is the leading supplier of electronic design automation software for microwave, RF, high-frequency, high-speed digital, RF system, electronic system level, circuit, 3-D electromagnetic, physical design and device-modeling applications. More information is available at www.keysight.com/find/eesof.


About Keysight Technologies

Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.

# # #

Contact:

Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @KeysightJSmith

Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]

Connie Wong, Asia
+852 3197-7818
[email protected]