SANTA ROSA, Calif., Aug. 18, 2015
Keysight Technologies, Inc. (NYSE: KEYS) today announced a new software package for use with Keysight logic analyzers, the B4661A memory analysis software. The Keysight B4661A memory analysis software offers the industry's only functional-level compliance violation testing capability across DDR4 and LPDDR4 speed changes.
The new B4661A memory analysis software has a performance analysis option that provides powerful new trace overview and navigation features. The memory analysis software also offers DDR and LPDDR decoder options. With this software and a Keysight logic analyzer, digital designers can monitor DDR3/4 or LPDDR2/3/4 systems to identify elusive violations in protocol or bus-level timing.
"Our customers who work with computer and embedded memory systems have asked for compliance tools that track compliance violations across speed changes and provide enhanced overviews of system performance," said Dave Cipriani, vice president and general manager of Keysight's Oscilloscope and Protocol Division. "With the new memory analysis software, customers can quickly identify design problems, allowing them to get products into the marketplace faster."
The memory analysis software includes four options:
The DDR decoder covers DDR/2/3/4 and provides protocol decoding of memory transactions using a Keysight logic analyzer. The protocol-decoding software translates acquired signals into easily-understood colorized bus transactions showing associated data bursts for double-edge data rate captures. The Keysight U4154B logic analyzer is already proven to capture DDR4 at 3.3 Gbps using the FS2510AB DDR4 DIMM interposer from a Keysight channel partner, FuturePlus Systems. The logic analyzer solution is ready to capture higher data rates when DDR4 standards incorporate higher data rates.
Using the LPDDR decoder, engineers can decode valid read and write commands to include row and column addresses and the complete data burst associated with the command. Keysight U4154B logic analyzers are proven to capture LPDDR4 at 3.2-Gb/s data rates.
Using the DDR3/4 and LPDDR2/3/4 performance analysis tool, navigation to problem areas is simplified with a powerful new traffic overview that presents the logic analyzer trace capture at a high level with user-selected filtering.
Keysight will showcase its new memory analysis software for computer and embedded DDR3/4 and LPDDR2/3/4 memory applications and new data import tool at the Intel Developer Forum, San Francisco, Aug. 18–21 and at MemCon, Santa Clara, Calif., Oct. 13.
Additional information about Keysight's B4661A memory analysis software is available at www.keysight.com/find/B4661A. Images are available at www.keysight.com/find/B4661A_images.
Keysight offers a complete logic analyzer portfolio of instruments with a variety of form factors to meet customer needs.
U.S. Pricing and Availability
Keysight Technologies' memory analysis software can be ordered now, with shipments planned for November. Prices start at $4,000.
The new test suite is recommended for use with Keysight's 4.0-Gb/s U4154B logic analysis module. More information is available at www.keysight.com/find/U4154B.
Keysight Software
Keysight software is downloadable test and measurement expertise. From first simulation through first customer shipment, Keysight software tools enable engineering teams to accelerate from data to information to actionable insight. Visit www.keysight.com/find/software to learn more and view the recently received 2014 Market Leadership Software Instrumentation award from Frost & Sullivan. Download free software trials at www.keysight.com/find/free_trials.
Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]