SANTA ROSA, Calif., March 20, 2015
Keysight Technologies, Inc. (NYSE: KEYS) today announced a new option for its industry-leading 89600 VSA software, enabling standard-compliant downstream modulation analysis of version 3.1 of the Data Over Cable Service Interface Specification (DOCSIS 3.1). Option BHM provides decoding of physical-layer link channel (PLC) information and measurements of modulation error ratio (MER) and bit error rate (BER).
Currently, the option supports a variety of Keysight measurement platforms, including two that offer bandwidth greater than 192 MHz: the N9040B UXA X-Series signal analyzer and the U5303A PCIe 12-bit high-speed digitizer. The UXA, which is Keysight's flagship signal analyzer, provides the highest MER performance at all DOCSIS frequency bands over a wide power range. The U5303A is a lower-cost alternative that provides excellent MER.
"As the gold standard for demodulation and analysis of today's most complex signals, the 89600 VSA software is an indispensable tool for designers working on the forefront of cable technology," said Satish Dhanasekaran, marketing manager of Keysight's Microwave and Communications Division. "With these new capabilities, developers will be able to more thoroughly verify the performance of today's complex, high-speed components, chipsets and set-top boxes."
With the DOCSIS 3.1 option, the 89600 VSA software provides post-processing analysis of PLC-coded, standards-compliant downstream signals. The software extracts the next codeword pointer (NCP) from acquired signals, creates the necessary OFDM map and demodulates DOCSIS 3.1 signals. It can then measure MER and BER and accumulate long-term results.
Developers can also use a separate option, BHF, custom OFDM modulation analysis, to characterize MER in upstream or downstream signals. This flexible diagnostic tool allows measurement and analysis of non-standard DOCSIS 3.1 signals with the full complement of capabilities in the 89600 VSA software.
The 89600 VSA software is a comprehensive set of tools for demodulation and vector signal analysis. These tools enable developers to explore virtually every facet of a signal and optimize their most advanced designs.
U.S. Pricing and Availability
Option BHM, DOCSIS 3.1 modulation analysis for 89600 VSA software, can be ordered now at a list price of $10,000 and a typical configured price of $18,606.
More information is available online at http://www.keysight.com/find/89600vsa. High-resolution product images are available at www.keysight.com/find/89600vsa_images.Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com