302 Moved Temporarily

This document you requested has moved temporarily.

It's now at https://localhost:8955/main/header.jspx?curr_url=http://about.keysight.com/en/newsroom/pr/2015/21jan-em15014.shtml?cc=US&myAgilentEmail=&section=bd&lc=eng&cc=MU.

Keysight Technologies Extends UXM Wireless Test Set LTE-A Carrier Aggregation Support with 3CC, TDD, Uplink Measurements

  
  

SANTA ROSA, Calif., Jan. 21, 2015

Keysight Technologies, Inc. (NYSE: KEYS) today announced expanded capabilities for the E7515A UXM wireless test set. The new features address the rapidly evolving 3GPP LTE-Advanced carrier aggregation advancements.

The UXM wireless test set is a highly integrated signaling test set created for functional and RF design validation in the 4G era and beyond. The UXM supports multiple cells, downlink and uplink carrier aggregation, MIMO up to 4x2 and integrated fading – allowing users to assess design readiness with greater confidence.

The E7515A UXM wireless test set update provides:

  • Chipset and UE designers the ability to validate 450 Mbps downlink end-to-end IP data throughput (by aggregating three 20 MHz component carriers) allowing mobile operators to use limited bandwidth resources for increased end-user download speeds
  • Verification of 100 Mbps uplink data rates via 2CC uplink carrier aggregation for both FDD and TDD, as well as intra-band measurement results using the industry-proven X-Series measurement applications
  • Leading-edge features for a multitude of UE test applications, including RF, data throughput, mobility, battery drain, functional and OTA
  • Further enhancements for device validation, such as eICIC, 64QAM uplink modulation and multi-cell mobility

"This new update adds the cutting-edge capabilities customers will need to address the latest, and evolving, wireless device validation and test requirements," said Joe DePond, general manager of Keysight's Mobile Broadband Operation. "The UXM's powerful and flexible platform architecture allows us to address these new requirements and future requirements of the latest high-performance LTE-Advanced chipset and UE designs."

More information about Keysight's UXM wireless test set is available at www.keysight.com/find/UXM. High resolution images are available at www.keysight.com/find/UXM_images. Videos demonstrating the UXM's versatile capabilities are available on YouTube. Contact Keysight at www.keysight.com/find/contactus for E7515A UXM pricing and delivery information.
About Keysight Technologies

Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.

# # #

Contact:

Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith

Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com

Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com