Keysight Technologies Introduces World's Only 50 GHz PXIe Vector Signal Analyzer

  
  

New VSA Provides Industry's Fastest, Low-Level Spur Searching Capability on the Market for Satellite Test

Highlights:

  • Highest PXI VSA frequency coverage for mmWave measurement and analysis
  • Superior sweep speed to reduce test time
  • Excellent dynamic range for analysis of low-level signals

SANTA ROSA, Calif., Oct. 27, 2015

Keysight Technologies, Inc. (NYSE: KEYS) today introduced a 50 GHz frequency extension to the M9393A PXIe performance vector signal analyzer (VSA), providing frequency coverage previously unseen in modular instrumentation. With coverage of Ka-band frequencies and beyond, the M9393A delivers Keysight's proven millimeter wave (mmWave) measurement technology in a PXI form factor for manufacturing and design validation of modems, transponders and sub-components for commercial and military satellite communications.

The innovative design of the M9393A offers engineers the ability to validate the performance of Ka-band designs with continuous frequency sweeps from 3.6 to 50 GHz (option FRX) and direct access to 800 MHz of IF bandwidth (option WB1). With displayed average noise level (DANL) better than -155 dBm/Hz at 40 GHz and accelerated sweep speed, the M9393A provides the fastest low-level spur searching capability on the market. The compact, modular form factor allows for dual channel configuration in a single chassis for increased measurement density and time synchronous multi-channel radio frequency measurements.

"Satellite communication system designers are utilizing the 26.5 to 40 GHz Ka-band to enable high-throughput data links," said Mario Narduzzi, marketing manager of Keysight's Communications Measurement Solutions Division. "The M9393A's 50 GHz frequency extension, wideband IF output and industry-leading spur search capabilities provide unmatched speed to insight for satellite communications developers."

The M9393A's extremely low noise floor in Ka-band, combined with Keysight's 89600 VSA software enables measurements of 20 GHz of spectrum with -110 dBm DANL, in less than 10 seconds, for the fastest measurements of low-level harmonics and spurs. This fundamental test is not only a regulatory requirement, it is a key indicator of system performance, and often a bottleneck in testing. In the past, this measurement has required the test engineer to tradeoff coverage and time, with tests taking minutes to hours. The M9393A's frequency sweep speed eliminates this tradeoff and allows developers to track minute signal distortions that were previously not practical to examine. 

Upgradeable capability, including frequency, analysis bandwidth, number of channels and memory, allows engineers to quickly adapt to changing test needs, reducing overall cost of test. The extensible modular architecture of the M9393A allows for easy addition of the M9169E PXI-h switchable input programmable attenuator module, recommended for low noise, high reliability power control up to 50 GHz. The M9169E also enables automatic routing of the M9393A's built-in calibrator signal, improving amplitude accuracy and uptime.

U.S. Pricing and Availability

The M9393A with options FRX and WB1 are now available for order, with prices starting at $77,000.

The M9169E is now available for order, starting at $12,000.

More information will be available at www.keysight.com/find/M9393A and www.keysight.com/find/M9169E. High-resolution images are available at www.keysight.com/find/M9393A_images.

About Keysight in Modular

Keysight provides unrivaled PXI and AXIe performance built on the industry's most accurate measurement science. Keysight helps engineers get to first measurement faster with common measurement software and Keysight Reference Solutions. Keysight has the industry's largest global network of experienced application engineers and metrology-grade calibration centers. Additional information about Keysight's PXI and AXIe modular test and measurement solutions is available at www.keysight.com/find/modular.


About Keysight Technologies

Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2014. Information about Keysight is available at www.keysight.com.

# # #

Contact:

Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @KeysightJSmith

Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]

Connie Wong, Asia
+852 3197-7818
[email protected]