302 Moved Temporarily

This document you requested has moved temporarily.

It's now at https://localhost:8955/main/header.jspx?curr_url=http://about.keysight.com/en/newsroom/pr/2015/30nov-nrb15168.shtml?cc=US&myAgilentEmail=&section=bd&lc=kor&cc=KR.

Keysight Technologies, UCSD, Demonstrate World's First 5G, 100 to 200 Meter Communication Link up to 2 Gbps

  
  

64- and 256-Element Phased-Array Beam-Pointing Communication Link Focused on Applications for 5G 60-GHz Communication Systems with Beamforming Capabilities and the Aerospace & Defense Industry

Highlights:

  • Proves the viability of a 5G communication link with Gbps data-rate performance
  • Uses UCSD’s 64- and 256-element phased-array system-on-a-chip

SANTA ROSA, Calif., Nov. 30, 2015

Keysight Technologies, Inc. (NYSE: KEYS), in collaboration with The University of California, San Diego (UCSD), has demonstrated the world's first 64 (8 x 8) and 256-element (16 x 16), 60-GHz silicon wafer-scale phased-array transmitter with integrated high-efficiency antennas for Gbps communications at 100 to 200 meters. With this demonstration, Keysight and UCSD have now proven that a 5G communication link is not only possible, but can deliver record performance.

Keysight's collaboration with UCSD builds on an earlier effort between the university and TowerJazz, which resulted in development of the industry's first 64- and 256-element system-on-a chip (SoC) phased arrays operating at 60-GHz. Each wafer-scale SoC comprises a 60-GHz source, amplifiers, distribution network, phase shifters, voltage controlled amplifiers and high-efficiency on-chip antennas. The chips were designed to meet the needs of 5G high-performance Gbps data-rate communication systems with beamforming capabilities and for Aerospace & Defense systems.

Following the development of the phased-array SoCs, Keysight and UCSD set out to prove they could be used in a communications link. All work was sponsored by the Defense Advanced Research Projects Agency (DARPA) and Keysight.

To develop that link, UCSD relied on a powerful suite of Keysight instruments that included the M8190A arbitrary waveform generator, E8267D PSG vector signal generator and the DSOS804A Infiniium S-Series high-definition oscilloscope with 10-bit ADC. For local oscillator generation, the Keysight E8257D PSG analog signal generator was employed.

The 60-GHz 802.11ad waveform UCSD required for the development effort was generated using Keysight's Signal Studio software and analyzed using its 89600 VSA software. Keysight's 81199A Wideband Waveform Center software also proved valuable, helping UCSD link transmit and receive, apply digital pre-distortion and improve error-vector-magnitude.

"UCSD, a world leader in low-cost SiGe and CMOS phased-arrays, has demonstrated several phased-array systems operating in the 6- to 100-GHz range and developed the first affordable wafer-scale 64- and 256-element phased-array transmitter for 5G communications," said Gabriel M. Rebeiz, distinguished professor and wireless communications industry chair at UCSD.

"The Keysight suite of equipment and software, with its ease of use and technical support, proved essential to enabling the rapid demonstration of the 100-200 meter 802.11ad and 5G link and allowing our phased-array to scan +/-45 degrees in all planes," said Dr. Samet Zihir, post-doctoral fellow at UCSD. "We are very happy to have partnered with Keysight on this project, and we look forward to using this equipment and software suite on networked 5G systems."

"Keysight is actively involved in 5G standards development and is fully committed to innovating the solutions needed to accelerate deployment of the next generation of wireless communications," said Mark Pierpont, vice president and general manager Keysight's Communications Measurement Solutions. "That's why we are so proud to have collaborated with UCSD on the 5G communication link. It not only represents a significant advance in the realization of 5G, but also paves the way for future research and development of millimeter-wave communication systems."

All Keysight instrumentation and software used in the development of the 5G communication link is available now. The phased-array SoCs are also now available. An image of the phased array and Keysight equipment suite is available at www.keysight.com/find/5GCommLink_images.

For additional information about the 5G communication link research at UCSD, contact professor Gabriel M. Rebeiz, Department of Electrical and Computing Engineering at UCSD, +1 858 336 3186 or rebeiz@ece.ucsd.edu.

About UCSD

The University of California, San Diego, is one of the leading universities in mixed-signal, microwave and mm-wave RFICs, digital communications, applied electromagnetics, optics and nano-electronics research, and is home to the Center for Wireless Communications. UC San Diego recently ranked 5th in the nation with an annual research budget exceeding $1 billion. The UC San Diego Jacobs School of Engineering ranks #7 in the USA according to the U.S. News & World Report best global universities ranking published in Oct. 2015. The Electrical and Computer Engineering Department is led by 56 faculty and trains more than 500 graduate students per year. For more information, please visit www.ece.ucsd.edu and www.ucsd.edu.

About Keysight in 5G

The development of 5G depends on up-to-date tools that let designers easily explore new signals, scenarios and topologies. Keysight's 5G solutions are ready to enable deeper insights as development evolves with the standard. In design and test, Keysight is enabling industry leaders to innovate across new and existing technologies as they transform ideas into reality. Additional information about Keysight's 5G design, test and measurement solutions is available at www.keysight.com/find/5G.


About Keysight Technologies

Keysight Technologies (NYSE:KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2015. Information about Keysight is available at www.keysight.com.

# # #

Contact:

Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith

Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com

Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com