Highlights:
- New swept source optical coherence tomography options now support up to 1 GS/s on the 12-bit high-speed data acquisition PCIe card
- Faster image acquisition up to 200 kHz A-scan rate, continuously
- Targeting applications in various non-invasive medical imaging
SANTA ROSA, Calif., April 4, 2016
Keysight Technologies, Inc. (NYSE: KEYS) today introduced swept source optical coherence tomography (SS-OCT) application options running at 1 GS/s (-SS2) and 500 MS/s (-SS1). The new options, now available on the U5303A high-speed data acquisition PCIe card, enable OEMs to obtain faster image acquisition by increasing sampling rate and A-scan rate. This allows for non-invasive, high-speed medical imaging in various applications, including ophthalmology, dermatology, gastrointestinal endoscopy, intravascular imaging, oncology and angiography.
This real-time processing solution allows OEMs to develop their SS-OCT engine using the development environment provided, which includes a GUI and C++. Furthermore, the options support "up and down sweep" and "up-sweep only", including improved trigger accuracy for targeting phase sensitive applications and a FFT phase readout.
The new options also ensure improved SFDR due to new x4 (-SS2) and new x2 (-SS1) oversampling interpolation and guarantee SS-OCT synchronization for A-scan and B-scan trigger, enabling better image clarity and quality. Moreover, swept source maximum analysis depth is independent of the k-clock frequency, allowing adjustment of the maximum depth range being done by changing sample rate. Differences between the k-clock and OCT optical path can be compensated electronically with a programmable delay of ±64 ns.
"These new SS-OCT options enables usage of a fast acquisition running up to 200 kHz scan rate," said Daniel Aebischer, special OEM applications project manager for digitizers, Keysight's Communications Solutions Group. "This capability is critical in some applications, such as cardiovascular when the blood stream has to be interrupted in order to take the measurement. Increasing speed is essential even in gastrointestinal, endoscopic applications when continuous acquisition is required to sustain the data flow."
Both -SS2/-SS1 options are available on the Keysight U5303A, a compact dual-channel ADC card delivering high dynamic range and high effective number of bits (ENOB) for enhanced image quality. As part of the OEMs development tool environment, a dedicated OCT GUI with C++ API and Labview support are provided.
The real-time SS-OCT processing engine was developed using Keysight's U5340A FPGA development kit. OEMs also can develop their own real-time processing engine. This gives way to reusability from one ADC technology to another.
Our hardware allows OEM to see smaller and deeper by preserving the signal integrity and detecting the smallest signals, whilst our complete offering minimizes risks with ease of integration and reduces time-to-market.
Information about product configuration is available at www.keysight.com/find/U5303A. High-resolution images are available at www.keysight.com/find/SS-OCT_PCIe_Digitizer_images.
Pricing and Availability
The applications options dedicated to swept source optical coherence tomography (-SS2/-SS1) are available now on the U5303A 12-bit PCIe high-speed digitizers. Please contact digitizers@keysight.com for more information.
About Keysight High-Speed Digitizers
Keysight high-speed digitizers are the result of more than 300 years of cumulative research and development experience in analog-to-digital conversion technology. This ensures the ability to achieve the most effective and reliable analog-to-digital conversion at high-resolution and fast sampling rates. Information on the technology and its applications is available at www.keysight.com/find/high-speed-digitizers.
About Keysight in Modular
Keysight provides unrivaled PXI and AXIe performance built on the industry's most accurate measurement science. Keysight helps engineers get to first measurement faster with common measurement software and Keysight Reference Solutions. Keysight has the industry's largest global network of experienced application engineers and metrology-grade calibration centers. Additional information about Keysight's PXI and AXIe modular test and measurement solutions is available at www.keysight.com/find/modular.
Keysight Technologies (NYSE: KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2015. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com