Highlights:
- Automates testing of 100G four-lane attachment unit interface (CAUI-4) applications
- New apps operate on real-time and equivalent-time (sampling) oscilloscopes
- Generate comprehensive pass/fail reports in minutes
SANTA ROSA, Calif., May 6, 2016
Keysight Technologies, Inc. (NYSE: KEYS) today introduced the industry's most comprehensive compliance application software for testing electrical characteristics of 100G four-lane attachment unit interface (CAUI-4) networking applications. The software supports the IEEE 802.3bm standard, which accommodates optical networking advances and enables higher density applications.
The new Keysight N8841A CAUI-4 compliance software application (for real-time Infiniium Z-Series oscilloscopes with 63 GHz bandwidth) and the N1082A-4TP CAUI-4 compliance software application (for 86100D DCA-X sampling oscilloscopes) help network design engineers accelerate turn-on and debug of 100G Ethernet networking systems. Automatic execution of physical layer tests ensures accurate results while reducing test times from hours to minutes.
Increased network testing needs result from growing consumer demand for more bandwidth from network hardware. 100G Ethernet is leading the way to larger bandwidth across network backbones and data center networking.
The N8841A and N1082A-4TP software applications provide automated test scripts that allow quick and reliable testing of chip-to-chip and chip-to-module channels at specified test points. Engineers can automate both software applications to run over extended periods of time as well as add their incremental user-defined tests if desired.
The N8841A works with Infiniium Z-Series oscilloscopes with 63 GHz of bandwidth. These scopes feature the industry's lowest noise and jitter measurement floors as well as higher timing resolution, which is achieved through a fast and responsive sample rate of 160 GSa/s.
The N1082A-4TP works with 86100D DCA-X oscilloscopes. This scope combines low-noise, high-bandwidth receivers with an acquisition system that is particularly well suited for accurate characterization of high-speed digital signals. The N1082A-4TP's measurement capabilities are supported by a variety of DCA plug-in modules, such as the 86108B 50-GHz precision waveform analyzer module; N1045A 60-GHz module; or N1055A 50-GHz TDR/TDT module.
Additional information about Keysight's N8841A CAUI-4 and N1082A-4TP CAUI-4 compliance applications is available at www.keysight.com/find/N8841A and www.keysight.com/find/N1082A. Images are available at www.keysight.com/find/CAUI-4_images.
U.S. Pricing and Availability
The Keysight N8841A CAUI-4 compliance software application for real-time oscilloscopes and the Keysight N1082A-4TP CAUI-4 compliance software application for sampling oscilloscopes are priced at $8,280 each. The N8841A CAUI-4 compliance application for real-time oscilloscopes is compatible with all currently-shipping Infiniium real-time oscilloscopes that have 63 GHz bandwidth. The N1082A-4TP CAUI-4 compliance application for sampling oscilloscopes is compatible with all currently-shipping 86100D DCA-X model oscilloscopes.
About Keysight in Modular
Keysight provides unrivaled PXI and AXIe performance built on the industry's most accurate measurement science. Keysight helps engineers get to first measurement faster with common measurement software and Keysight Reference Solutions. Keysight has the industry's largest global network of experienced application engineers and metrology-grade calibration centers. Additional information about Keysight's PXI and AXIe modular test and measurement solutions is available at www.keysight.com/find/modular.
About Keysight in Software
Keysight software is downloadable design, test and measurement expertise. From first simulation through first customer shipment, Keysight software tools enable engineering teams to accelerate from data to information to actionable insight. Additional information is available at www.keysight.com/find/software Download free software trials at www.keysight.com/find/free_trials.
Keysight Technologies (NYSE: KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2015. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]