Highlights:
- Easily view and control the N8900APV Series PV Simulator from the control tab
- Quickly create and download photovoltaic I-V curves from the curve workspace tab
- Create static and dynamic EN50530 test reports with one click from the MPPT efficiency tab
SANTA ROSA, Calif., Sept. 7, 2016
Keysight Technologies, Inc. (NYSE: KEYS), the first company to introduce a one-box, 1,500 V, photovoltaic (PV) array simulation solution—the N8900APV Series—today announced the addition of automated static and dynamic maximum peak power tracking (MPPT) test to its Solar Array Simulator (SAS) Control software for N8900APV Series PV simulators. The static and dynamic MPPT tests are performed in accordance with the European Standard EN50530 (April 2010) procedure, which is widely accepted as the industry standard for the overall efficiency of grid-connected photovoltaic inverters. This update to the software also includes integration with the Keysight BenchVue platform.
The Keysight SAS Control software is a no-cost way for PV/solar inverter designers to control their N8900APV Series Photovoltaic Array Simulators in order to test the MPPT of their inverters. The software allows the user to control the N8900APV's output as well as easily create, visualize and download PV/solar I-V curves to the instrument using the intuitive curve workspace. After a designer downloads a curve to an N8900APV, they can enable the output and watch as their PV inverter searches for the maximum power point to gain insight into their MPPT algorithm.
"The European standard EN50530 gives photovoltaic inverter designers a standard way to evaluate their maximum peak power tracking algorithms and compare them to their competitors—however, implementing this test standard can be quite challenging and time consuming,” said Siegfried Gross, general manager of Keysight's Automotive and Energy Solutions (AES) group. "Under our new organizational structure announced last November, Keysight has aligned the company's activities around the development of solutions to our customers' most challenging problems. Our PV simulation solution is just one of many solutions to come under this new structure.”
After the built-in, 30-day free trial, users can purchase a Pro license of the SAS Control software (DG8901A). In addition to all the benefits and features of the no-cost version, SAS Control Pro permanently adds the automated static and dynamic EN50530 MPPT test capability. Designers can simply input the test parameters, such as Pmp, Vmp, etc., click Start Test, and the software does the rest. Once the test is complete, SAS Control Pro creates a report formatted to the EN50530 standard, as well as a detailed log file with all of the measurements from the test.
U.S. Pricing and Availability
All products are orderable and available immediately. The pricing is as follows:
Additional Information
More information about the Keysight N8900APV Series photovoltaic array simulators is available at www.keysight.com/find/N8900APV. More information about the SAS Control software for the N8900APV photovoltaic array simulators is available at www.keysight.com/find/SasControlSoftware.
High-resolution product images are available at www.keysight.com/find/N8900APV_images. Videos about the test solution are available on YouTube at https://www.youtube.com/playlist?list=PL2XuMA5AwNUwYj7oLO84xp-Kk0o-cW_1P.
Keysight Technologies (NYSE: KEYS) helps customers bring breakthrough electronic products and systems to market faster and at a lower cost. Keysight's solutions go where the electronic signal goes, from design simulation, to prototype validation, to manufacturing test, to optimization in the network. Customers span the worldwide communications ecosystem, internet infrastructure, aerospace & defense, automotive, semiconductor and general electronics end markets. Keysight generated revenues of $2.9B in fiscal year 2015. More information is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com