Highlights:
- Full bandwidth (12 GHz) browsing solution for Keysight’s InfiniiMax I/II probes
- Unparalleled signal fidelity measurement with extremely low probe loading
- Unmatched usability with thumbwheel-controlled tip span and replaceable spring-loaded tips
SANTA ROSA, Calif., March 16, 2016
Keysight Technologies, Inc. (NYSE: KEYS) today introduced the N2839A differential browser head for use with InfiniiMax I/II Series probe amps, bringing the measurement fidelity of a solder-in probe head to hand-held browsing. When used with the InfiniiMax II 1169A probe amplifier, the N2839A gives users 12 GHz of bandwidth, making this the world's most usable hand-held browser solution for measuring high-speed differential or single-ended signals.
The spring-loaded probe tips of the N2839A ensure a secure connection to the DUT. The probe tips can be adjusted to accommodate targets from 0 mm to 3 mm apart using the thumbwheel and can be easily and quickly replaced if accidental damage occurs. The low-inductance ground spring ensures that the probe's frequency response remains constant regardless of the span range setting.
Unlike conventional probe browsers in this class, the N2839A provides extremely low probe loading. As the signal speed increases, the capacitance element of the probe's input becomes a dominant factor in determining the amount of probe loading. The larger the input capacitances, the more the probe may load the DUT or affect the response of the measurement when the measured frequency increases. The N2839A provides 0.21 pF of low input capacitance, which is just as low as that of a solder-in head, minimizing the probe effect in measuring high-speed signals.
"Our design goal for the new N2839A browser was to deliver a high-quality, durable, differential browser head that has the signal fidelity of our solder-in probe-heads," said Dave Cipriani, vice president and general manager of Keysight's Oscilloscope and Protocol Division. "This combination gives our customers an easy-to-use probe with excellent measurement accuracy."
Additional information about Keysight's new InfiniiMax II browser head is available at www.keysight.com/find/n2839a. Product images are available at www.keysight.com/find/N2839a_images.
U.S. Pricing and Availability
Keysight N2839A browser head can be ordered today at the prices listed below. Limited shipments will begin in March 2016.
Model | Description | Price |
N2839A | InfiniiMax II browser head | $2,700 |
N2837A | InfiniiMax II browser tip kit | $150 |
About Keysight in Digital Test
Keysight's solutions for digital applications are driven and supported by Keysight experts who are involved in various international standards committees. Keysight experts are active in the Joint Electronic Devices Engineering Council (JEDEC), PCI Special Interest Group (PCI-SIG®), Video Electronics Standards Association (VESA), Serial ATA International Organization (SATA-IO), USB Implementers Forum (USB-IF), Mobile Industry Processor Interface (MIPI®) Alliance, Ethernet standards (IEEE 802.3), Optical Internetworking Forum (OIF) and many others. Keysight is committed to involvement in standards groups and related workshops, plugfests and seminars to ensure the right test solutions are created to meet customers' evolving needs.
Keysight Technologies (NYSE: KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2015. Information about Keysight is available at www.keysight.com.
# # #
PCI-SIG® is a registered trademark of PCI-SIG. MIPI® service marks and logo marks are owned by MIPI Alliance, Inc. and any use of such marks by Keysight Technologies is under license. Other service marks and trade names are those of their respective owners
Contact:
Janet Smith, Americas
+1 970 679 5397
janet_smith@keysight.com
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
sarah_calnan@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com