Highlights:
- New high current ultra low noise filter now covers up to 500mA with keeping 10 μVrms noise performance
- World's only ultra low noise power source available for under $10K
SANTA ROSA, Calif., May 17, 2016
Keysight Technologies, Inc. (NYSE: KEYS) today introduced a new high current ultra low noise filter for the B2961A and B2962A 6.5 Digit Low Noise Power Source that can supply up to 500 mA while maintaining 10 μVrms and 1nVrms/√Hz (at 10 kHz) noise performance. With a starting price of less than $10K, the B2961A and B2962A are the world's only low-cost standalone power sources capable of sourcing at ultra-low noise levels. These products help researchers, electronic development engineers and electronic technicians to meet their most difficult measurement challenges during device development and evaluation.
As electronic equipment and devices become smaller, integrated and more portable, they demand greater intelligence, integration, miniaturization and lower-power consumption. Researchers, designers and developers pursuing the innovations and breakthroughs needed to develop these next-generation devices typically require basic equipment such as power supplies and sources for this work. When sensitive devices are being developed, those sources must have high precision and resolution, as well as low-noise voltage.
Keysight's B2961A and B2962A deliver the best-in-class precision and extremely low noise floors that today's design engineers researching and developing AD/DA converters, VCOs, sensors and transducer devices demand. Such devices often require wide current and voltage coverage with low noise. With its new ultra low noise filter, the B2961Aand B2962A can now output up to 500 mA while still maintaining an extremely low-noise floor of 10 μVrms and 1nVrms/√Hz (at 10 kHz). These capabilities make it the ideal precision source for use with other instruments such as network analyzers, signal source analyzer and nano-voltmeters.
Most signal source analyzers, even those with a built-in source, cannot simultaneously supply a low-noise voltage output at the current levels needed for many engineering applications. However, the B2961A and B2962A's new high current ultra low noise filter meets both of these requirements.
"Accurate development and evaluation of sensitive electronic devices requires power sources with high precision, high resolution, and ultra-low noise," said Masaki Yamamoto, general manager of Keysight's Hachioji Semiconductor Test Division. "With the B2961A and B2962A's enhanced high current ultra low noise filter, customers now get optimal flexibility in one power source to address even their toughest measurement challenges. Moreover, its low starting price makes it easily accessible to users working on a wide range of applications, whether analog IC companies, foundries or IDMs, just to name a few."
More information about Keysight's enhanced B2961A and B2962A ultra low noise power sources is available at www.keysight.com/find/PrecisionSource. Images of the new power sources are available at www.keysight.com/find/PrecisionSource_images.
U.S. Pricing and Availability
Keysight's enhanced B2961A and B2962A ultra low noise power sources are available today at a starting price of $6,963.
Keysight Technologies (NYSE: KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2015. Information about Keysight is available at www.keysight.com.
# # #
Contact:
Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @KeysightJSmith
Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]