Keysight Technologies Introduces the Industry's Only 10 GS/s, DC Coupled, 10-bit PCIe® High-Speed Digitizer

  
  

Unique Digitizer Combines High Performance in a Very Small Form Factor

Highlights:

  • New 10 GS/s high-speed digitizer
  • 10-bit resolution, DC up to 2.5 GHz bandwidth, very small form factor
  • Ideal for applications requiring a high sampling rate and a large bandwidth, such as medical research, MS-TOF, LiDAR, NDT and DSTS

SANTA ROSA, Calif., May 31, 2016

Keysight Technologies, Inc. (NYSE: KEYS) today launched the U5310A 10-bit PCIe® high-speed digitizer running at 10 GS/s. With its very-high dynamic range and 10-bit resolution across a wide 2.5 GHz bandwidth, the high-speed digitizer allows the capture of fast transients with high fidelity.

This unique ADC card is designed for embedded OEM applications, such as medical research, analytical time-of-flight (MS-TOF), environmental monitoring (LiDAR), ultrasonic non-destructive testing (NDT), semiconductor testing and distributed strain temperature sensor (DSTS). Furthermore, the U5310A is ideal for advanced physics experiments using single-shot or event-based applications.

The new U5310A high-speed digitizer features two channels with 10-bit resolution, simultaneous sampling at up to 5 GS/s, and an unrivaled 10 GS/s in interleaved mode. With a DC up to 2.5 GHz bandwidth, this digitizer provides on-board real-time averaging at full sampling rate and large 4 GB memory.

Keysight developed new proprietary ICs for the U5310A. In particular, the low distortion and low noise LDNA front-end amplifier IC to drive the ADC. This key component provides single ended to differential outputs with a distortion from 10 to 15 dB lower than the distortion of the ADC—therefore overall performance is not impacted.

Keysight also designed a low noise dedicated QMCK clock IC with very low 25 fs jitter. This specific IC drives the two ADCs, minimizing jitter. Moreover, the TRAC trigger IC provides time precision of 15 ps RMS.

"With its new design and outstanding performance, such as exceptional signal-to-noise ratio, minimum overshoot and flat frequency response, the U5310A allows unequalled measurement capabilities for time and frequency domain applications," said Didier Lavanchy, high-speed digitizers manager, Keysight's Communications Solutions Group. "With its newly developed technologies, such as the proprietary ICs, the U5310A ensures better measurement fidelity with higher resolution—thus allowing customers to see what they couldn't see before".

The averager (-AVG) firmware ensures accumulation of a large number of triggers for synchronous real-time sampling at 5 GS/s on two channels and 10 GS/s when interleaved. Innovative features, such as the unique programmable self-trigger output, optimizes the signal-to-noise ratio and increases the ability to measure very small peaks accurately.

This new PCIe high-speed digitizer focuses on interoperability, reusability and upgradability with other U53xxA digitizers. The U5310A's software driver provides support for multiple programmable interfaces ensuring easy integration of the ADC card into existing environments.

Additional information about product configuration and pricing is available at www.keysight.com/find/U5310A. High-resolution images are available at www.keysight.com/find/U5310A_PCIe_Digitizer_images.

Price and Availability

The U5310A PCIe high-speed digitizer, 2-channel, 10-bit, up to 10 GS/s is available now. Contact Keysight at [email protected] for additional information.

About Keysight High-Speed Digitizers

Keysight's high-speed digitizers are the result of more than 300 years of cumulative research and development experience in analog-to-digital conversion technology. This ensures the ability to achieve the most effective and reliable analog-to-digital conversion at high-resolution and fast sampling rates. Information on the technology and its applications is available at www.keysight.com/find/high-speed-digitizers.

About Keysight in Modular

Keysight provides unrivaled PXI and AXIe performance built on the industry's most accurate measurement science. Keysight helps engineers get to first measurement faster with common measurement software and Keysight Reference Solutions. Keysight has the industry's largest global network of experienced application engineers and metrology-grade calibration centers. Additional information about Keysight's PXI and AXIe modular test and measurement solutions is available at www.keysight.com/find/modular.


About Keysight Technologies

Keysight Technologies (NYSE: KEYS) is a global electronic measurement technology and market leader helping to transform its customers' measurement experience through innovations in wireless, modular, and software solutions. Keysight's electronic measurement instruments, systems, software and services are used in the design, development, manufacture, installation, deployment and operation of electronic equipment. The business had revenues of $2.9 billion in fiscal year 2015. Information about Keysight is available at www.keysight.com.

# # #

PCIe® is a U.S. registered trademark of PCI-SIG.

Contact:

Janet Smith, Americas
+1 970 679 5397
[email protected]
Twitter: @KeysightJSmith

Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]

Connie Wong, Asia
+852 3197-7818
[email protected]