Keysight Technologies Delivers Insight in 5G, IoT, Aerospace and Defense Design, Test Solutions at IMS 2017

  
  

Keysight experts will address pre-5G, 802.11ax, battery drain, drone detection and more

Highlights:

  • Learn how to streamline 5G design verification at 28GHz and 37-39GHz with new wideband signal source and analyzer families, along with the latest 5G application software
  • Learn how broadband millimeter-wave network analysis offers a breakthrough in traditional active device characterization and modeling in on-wafer and connectorized applications
  • Learn how to reduce your total cost of test and program costs with reliable satellite solutions
  • Learn how to maximize the life of small, on-board batteries with accurate battery drain measurements and understanding of power consumption patterns

SANTA ROSA, Calif., May 23, 2017

Keysight Technologies, Inc. (NYSE: KEYS) today announced it will demonstrate the latest design and test solutions for components and systems used in 5G communications, internet of things (IoT), and aerospace and defense applications that solve the toughest engineering challenges. Keysight, an IMS Gold Sponsor and 5G Summit Title Sponsor, will exhibit in Booth 1526, IEEE International Microwave Symposium, Hawaii Convention Center June 4–9.

Keysight's experts will be on hand to discuss simulation, design and test topics, including the following products and solutions.

  • The new Keysight N5290/91A broadband millimeter-wave network analyzer delivers unparalleled system-level accuracy from 900 Hz to 120 GHz. The analyzer produces metrology-grade results—enabling leading-edge developers to confidently characterize their millimeter-wave designs.
  • The PA/FEM test solution provides comprehensive, one-connection/multiple-measurement capability—enabling design engineers to measure modulation (ACPR, PAE, EVM) and CW characteristics (S-parameter, gain compulsion, P1dB) in 5G power amplifiers.
  • The IEEE 802.11ax life-cycle test solutions support WiFi BBIQ, 8x8 MIMO, OFDMA-MU UL/DL and their test coverage has been verified up to Draft 1.2 specification. The products enable WiFi chipset and 802.11ax device makers in simulation, design and verification, and volume production with industry-leading performance and cost of test.
  • The new SystemVue 2017 electronic system level (ESL) simulation software provides the industry's first Verizon 5G link level validation of 5G basestation and handset designs. The software integrates adaptive RF phased array MIMO beamforming in 5G mmWave channel environments with reference baseband modem and 28GHz RFIC architecture.
  • The FieldFox handheld microwave analyzers, which now connect to the 89600 VSA software, the industry's leading toolset for signal demodulation and vector signal analysis. The FieldFox to 89600 VSA link provides a powerful combination of hardware and software for design and troubleshooting of devices using signal formats such as APCO-25, TETRA, DSCR, emerging IoT, LTE, WCDMA, GSM and more.
  • The new multi-touch user interface (UI) for all models in the PNA Series of network analyzers. Updates to the UI include a 12.1-inch widescreen display, easy access to frequently used functions, and intuitive gestures to drag-and-drop or magnify traces.

Executive and technical session highlights include, "Testing 5G: OTA and the Connectorless World," "The Future of RF Semiconductor Test" and "Build-A-Beam for 5G and Radar - Designing and Simulating Phased Array Beamforming Systems." A complete list of executive and technical sessions is available at Keysight at IMS 2017.

About Keysight in 5G

The development of 5G depends on up-to-date tools that let designers easily explore new signals, scenarios and topologies. Keysight's 5G solutions are ready to enable deeper insights as development evolves with the standard. In design and test, Keysight is helping industry leaders innovate across new and existing technologies as they transform ideas into reality. Additional information about Keysight's 5G design, test and measurement solutions is available at www.keysight.com/find/5G.


About Keysight Technologies

Keysight Technologies is a leading technology company that helps its engineering, enterprise and service provider customers optimize networks and bring electronic products to market faster and at a lower cost. Keysight's solutions go where the electronic signal goes, from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $2.9B in fiscal year 2016. In April 2017, Keysight acquired Ixia, a leader in network test, visibility, and security. More information is available at www.keysight.com.

# # #

Additional information about Keysight Technologies is available in the newsroom at www.keysight.com/go/news and on Facebook, Google+, LinkedIn, Twitter and YouTube

Contact:

Geri Lynne LaCombe, Americas
+1 303 662 4748
[email protected]

Sarah Calnan, Europe
+44 (118) 927 5101
[email protected]

Connie Wong, Asia
+852 3197-7818
[email protected]