SANTA ROSA, Calif., April 4, 2018
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world, today announced iBypass DUO, the next generation bypass switch. iBypass DUO provides two management ports, as well as 10G and 1G support, which allows network security teams to switch inline security tools in and out of network without bringing down the network or creating a point of failure.
Today’s organizations face a myriad of network concerns including the increasing volume of multiprotocol traffic at higher data rates, mounting security threats, and a strict regulatory environment. Deploying inline security tools to inspect and control network traffic helps block incoming threats, but the same inline tools can complicate network operations and create potential points of failure. If an inline tool becomes unavailable, it can bring down the network link, significantly compromising network uptime and disrupting business continuity.
"With the increasing complexity of today’s networks, it is critical to ensure visibility for monitoring and security in inline deployments, " said Kevin Formby, vice president of market development at Keysight’s Ixia Solutions Group. "The ability to communicate with essential network elements at all times is ever more important, which is why Ixia developed the first bypass switch on the market with two management ports. "
In addition to the providing two management ports and 10G and 1G support, iBypass DUO uniquely offers users:
Like Ixia’s greater bypass switch portfolio, the iBypass DUO:
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $3.2B in fiscal year 2017. In April 2017, Keysight acquired Ixia, a leader in network test, visibility, and security. More information is available at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at www.keysight.com/go/news and on Facebook, Google+, LinkedIn, Twitter and YouTube.
Contact:
Geri Lynne LaCombe, Americas
+1 303 662 4748
[email protected]
Magda Antone, Europe
+34 (93) 3434612
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]