Keysight Launches Highly Scalable Channel Emulation Solution to Secure Performance of Mission Critical Tactical Wireless Communication Systems

  
  

Flexible PROPSIM MANET Channel Emulation Solution delivers end-to-end performance testing of MANET and mesh-network topologies

SANTA ROSA, Calif., June 4, 2018

Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world, today announced the PROPSIM MANET Channel Emulation Solution. This new solution secures end-to-end performance and interoperability of Mobile Ad-Hoc Networks (MANET) and mesh radio systems (a self-forming and self-healing reliable network that eliminates single points of failure) for tactical mission critical wireless communications.

Ensuring the robust inter-operation of avionics, surveillance, radar or satellite systems for mission critical wireless communications, manufacturers and military forces require the ability to test mixed networks that combine tactical and avionics radios with satellite links. Increased complexity and technological advancements, such as MIMO and beamforming in wireless military communication systems, has accelerated the need to test large mesh-network topologies with dynamically changing radio channel and interference conditions.

To address this need, Keysight has launched a high-performing, network level channel emulation solution that enables users to easily replicate field-testing conditions in a repeatable way. The PROPSIM MANET Channel Emulation Solution is a highly scalable and flexible solution that supports:

  • full mesh configurations of up to 64 radios using 4032 independent fading channels in a single unit for testing large SISO and MIMO mesh-network topologies,
  • up to 1.2GHz of instantaneous bandwidth for ultra-wideband support for testing gigabit links,
  • easy-to-use interface for dynamic scenario creation and for accessing all key radio channel parameters.

"The introduction of PROPSIM MANET Channel Emulation Solution enables designers of MANET and mesh radios to use a multipurpose tool that offers the flexibility they need to address a comprehensive set of tactical radio testing requirements," said Greg Peters, vice president and general manager of Keysight's aerospace & defense group. "This solution, in combination with Keysight's M8920A Radio Test Set, offers a complete platform for testing radios from simulation to manufacturing. As a result, designers have the confidence to ensure robust operation of any mission critical wireless communication system."


About Keysight Technologies

Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $3.2B in fiscal year 2017. In April 2017, Keysight acquired Ixia, a leader in network test, visibility, and security. More information is available at www.keysight.com.

# # #

Additional information about Keysight Technologies is available in the newsroom at www.keysight.com/go/news and on FacebookGoogle+LinkedInTwitter and YouTube.

Contact:

Geri Lynne LaCombe, Americas
+1 303 662 4748
[email protected]

Magda Antone, Europe
+34 (93) 3434612
[email protected]

Connie Wong, Asia
+852 3197-7818
[email protected]