SANTA ROSA, Calif., May 9, 2018
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world, today announced that Ixia, a Keysight Business, has collaborated with VMware to develop a solution that accelerates partner certification of network products to interoperate with the VMware NSX network virtualization platform.
The solution uses Ixia's IxNetwork to enable network equipment manufacturer (NEM) partners to self-certify their products with VMware NSX in a range of network topologies, helping them save significant costs while improving time-to-market.
VMware NSX delivers a completely new operational model for networking that forms the foundation of the Software-Defined Data Center. The NSX platform supports any IP-based underlay hardware, and the VMware NSX Technology Partner Program provides support and certification for the integration of partners' hardware switching and routing solutions with NSX. Ixia and VMware have worked together to develop and incorporate the required testing capabilities in the IxNetwork solution to facilitate the certification process for NEMs. Enterprises can then validate their network performance with the solution as well.
"Ixia has a strong reputation in network protocol and performance testing, and working with them has enabled VMware to significantly streamline the certification process for NSX partners," stated Umesh Mahajan, Vice President and General Manager of the NSX Platform at VMware. "The IxNetwork solution provides the performance and flexibility crucial to enabling our partners to interoperate with NSX in diverse customer environments. Ixia has been able to deliver a solution that we can use in our own labs, and be offered to our partners for deployment in their labs for new and ongoing certification testing in their own labs. We are pleased to be working with Ixia as we enhance the value of the NSX ecosystem."
IxNetwork provides VMware NSX partners advanced capabilities including Ixia's new Open vSwitch Database (OVSDB) Emulation. OVSDB is a management protocol for SDN environments used by the NSX controller to create hardware VXLAN Tunnel End Points (VTEP), and VXLAN encapsulation and de-encapsulation. Ixia's OVSDB Emulation eliminates the need for complex server infrastructure during testing.
"Ixia and VMware have collaborated to accelerate the self-certification network equipment manufacturers need to interoperate with VMware NSX," stated Scott Westlake, vice president of Business Development at Ixia Solutions Group, a Keysight Business. "Using IxNetwork, the NSX testing verifies control and data plane interoperability and performance, and provides optional scale testing during the development and certification phase. It offers NEM partners and enterprises the ability to test without the need to create very large, complex, and expensive server environments, improving their certification and accelerating their time-to-market."
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $3.2B in fiscal year 2017. In April 2017, Keysight acquired Ixia, a leader in network test, visibility, and security. More information is available at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at www.keysight.com/go/news and on Facebook, Google+, LinkedIn, Twitter and YouTube.
VMware and NSX are registered trademarks or trademarks of VMware, Inc. in the United States and other jurisdictions
Contact:
Geri Lynne LaCombe, Americas
+1 303 662 4748
geri_lacombe@keysight.com
Magda Antone, Europe
+34 (93) 3434612
press.emea@keysight.com
Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com