302 Moved Temporarily

This document you requested has moved temporarily.

It's now at https://localhost:8955/main/header.jspx?curr_url=http://about.keysight.com/en/newsroom/pr/2018/11jun-nr18057.shtml?cc=US&myAgilentEmail=&section=bd&lc=fre&cc=FR.

Keysight Technologies Delivers New USB Measurement Platform that Increases Efficiency in Design, Test, and Analysis

  
  

Streamline Series USB Platform offers advanced capabilities with zero compromises

SANTA ROSA, Calif., June 11, 2018

Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world, announced today a new measurement platform that ensures consistent, repeatable results across all phases of design. The new Keysight Streamline Series is comprised of compact USB instruments: vector network analyzers (VNAs), oscilloscopes and an arbitrary waveform generator (AWG) that leverage trusted Keysight technologies, measurement algorithms, and application software.

"The Keysight Streamline Series platform enables organizations to address the ever-increasing pressure to stay productive, optimize resources and meet tight deadlines in creating new electronic devices," said Dave Cipriani, vice president and general manager of Keysight's oscilloscope business. "Customers can now move confidently across every stage of their product lifecycle by leveraging accurate, repeatable results from whichever form factor they need: compact USB, modular, or benchtop."

Controlled via PC through a USB connection, Keysight's new instruments help customers save space on the test bench and are easily shared among members of a development team. The small rack size makes them ideal for manual or semi-automated testing in design-validation and light-manufacturing applications.

Keysight Streamline Series platform is available in three models:

  • The P937xA models are compact two-port VNAs with frequency coverage up to 26.5 GHz. All are designed to excel in the testing of passive devices such as antennas, filters and duplexers. Running on a host PC, the context-sensitive user interface is identical to that of Keysight's latest benchtop VNAs.
  • The P924xA high-performance oscilloscopes provide full measurement functionality along with advanced triggering, rapid waveform updates, and popular features such as zone triggering. With the Keysight InfiniiVision interface running on the user's PC, the look and feel is consistent with familiar benchtop oscilloscopes.
  • Using Keysight-exclusive Trueform waveform generation, the P9336A three-channel AWG provides 16-bit resolution with maximum analysis bandwidth of 540 MHz and maximum onboard memory of 4 GB. Applications range from general-purpose testing to complex I/Q signal generation for characterization of transceivers and modulators. To simplify signal creation, the USB AWG is compatible with Keysight Signal Studio software.

Additional Information

More information about Keysight Streamline Series instruments is available at www.keysight.com/find/streamline. Images are available at www.keysight.com/find/streamline-images.


About Keysight Technologies

Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor, and general electronics end markets. Keysight generated revenues of $3.2B in fiscal year 2017. In April 2017, Keysight acquired Ixia, a leader in network test, visibility, and security. More information is available at www.keysight.com.

# # #

Additional information about Keysight Technologies is available in the newsroom at www.keysight.com/go/news and on FacebookGoogle+LinkedInTwitter and YouTube.

Contact:

Geri Lynne LaCombe, Americas
+1 303 662 4748
geri_lacombe@keysight.com

Magda Antone, Europe
+34 (93) 3434612
press.emea@keysight.com

Connie Wong, Asia
+852 3197-7818
connie-ky_wong@keysight.com