SANTA ROSA, Calif., September 25, 2018
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world, announced the new, enhanced Keysight E8740A Automotive Radar Signal Analysis and Generation solution. This new solution enables radar-based, advanced driver assistance systems to proactively detect and mitigate risks of collisions.
As advanced driver-assistance systems (ADAS) and autonomous vehicles gain in popularity, they also raise concerns about safety and reliability. Autonomous vehicles are dependent on advanced sensor technology with highly integrated radar. According to the Society of Automotive Engineers (SAE), autonomous vehicles require up to 24 of these radar sensors in each car. Interference between sensors can seriously impact automotive radar reliability. Even a slight error or unexpected misbehavior in the system could lead to a critical situation or accident.
The new version of the Keysight E8740A automotive radar signal analysis and emulation solution is based on industry-leading, high-performance physical layer instruments to ensure best in class radio frequency (RF) and mmWave performance verification for each radar design under test, as well as an easy-to-use, intuitive user interface to ensure maximum productivity. This comprehensive test solution also generates various real-world conditions to address any potential automotive radar interference issues.
"Keysight understands that reliable technology is pivotal to minimize vehicle collisions, prevent human injuries, and ultimately save lives", said Siegfried Gross, vice president and general manager of Keysight's Automotive and Energy Solutions business unit. "That is why Keysight will continue to invest resources in this particular field as we aim to enable developers to overcome radar design and performance verification challenges."
The new Keysight E8740A automotive radar signal analysis and generation solution offers:
Additional information about Keysight's automotive test solutions is available at https://www.keysight.com/find/automotive and https://www.keysight.com/find/e8740a.
For images: www.keysight.com/find/automotive-radar-images
About Keysight Technologies
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $3.2B in fiscal year 2017. In April 2017, Keysight acquired Ixia, a leader in network test, visibility, and security. More information is available at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at www.keysight.com/go/news, Keysight blog, and on Facebook, Google+, LinkedIn, Twitter and YouTube.
Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662 4748
[email protected]
Fusako Dohi, Asia
+81 42 660-2162
[email protected]