SANTA ROSA, Calif., September 26, 2018
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world, announced it has extended the Ixia CloudLens visibility platform to provide packet-level visibility into virtual machine network traffic through Microsoft Azure Virtual Network Terminal Access Point (TAP).
Cloud adoption is nearly ubiquitous with 92 percent of companies reporting they have adopted the public cloud, according to the RightScale 2018 State of the Cloud Report. As cloud adoption increases, security concerns intensify. According to Gartner, clouds are secure, but organizations are often not using them securely1. Further, Gartner states that through 2022, at least 95% of cloud security failures will be the customer's fault2.
In a public cloud environment, traditional methods for gaining packet-level visibility can sometimes be challenging. Users typically installed sensors within their workloads for packet visibility. These agents/sensors compete for resources on the workload for operation and introduce added complexity.
The CloudLens Software-as-a-Service (SaaS) platform was designed from the ground up to retain the benefits of the cloud — elastic scale, flexibility, and agility, while enabling security, analytics, and forensics tools to acquire the needed packet-level data. CloudLens now offers an Azure feature that enables customers to mirror virtual machine network traffic which can then be filtered, replicated and forwarded to the appropriate analysis tools.
"Security is a shared responsibility between the cloud provider and the hosted organization, so we joined with Microsoft Azure and our technology partners to help our customers secure their clouds more effectively," said Scott Westlake, vice president, Alliances for Keysight's Ixia Solutions Group. "CloudLens enables customers to use the Microsoft Azure Virtual Network TAP to gain network traffic visibility and ensure the security and performance of their Azure cloud-based applications."
CloudLens provides a sensor that can be configured through API's from Azure Infrastructure as a Service (IaaS). This enables the user to forward network traffic to the CloudLens Sensor without the need to install a sensor in every workload.
"Deploying RSA NetWitness® Platform is critical to maintaining consistent security visibility across hybrid environments while customers are in the process of migrating workload to the cloud. Ixia CloudLens works with Azure's new Virtual Network TAP to streamline collection of the necessary packet level data from Azure instances for security monitoring and analysis via the RSA NetWitness Platform." — Matthew Chase, Senior Manager, Technical Alliances, RSA Security, LLC
"Wire data analysis is vital to monitor and manage applications migrated to Microsoft Azure for IaaS hosting, particularly in hybrid on-premises and cloud deployments. Ixia CloudLens, combined with Azure Virtual Network TAP, provides Dynatrace's Network Application Monitoring solution the complete visibility it needs in an easy to deploy and scalable way. This joint solution complements Dynatrace's agent-based solution for Azure native applications." — Krzysztof Ziemianowicz, Technology Strategist, Dynatrace
"Eastwind Networks offers customers ubiquitous breach analytics across public Cloud IaaS, private infrastructure, and SaaS. With data collection service powered by Ixia CloudLens, and in concert with Microsoft Azure Virtual Network TAP, our customers gain seamless access to the packet level data required for Eastwind to provide full context and detail into security breaches that occur on their Azure hosted workloads." — Paul Kraus, CEO, Eastwind Networks
CloudLens is available in the Azure Marketplace. Visit Ixia in booth #1448 at Microsoft Ignite, September 24-28 in Orlando, Florida to learn more about CloudLens and Azure Virtual Network TAP.
About Keysight Technologies
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $3.2B in fiscal year 2017. In April 2017, Keysight acquired Ixia, a leader in network test, visibility, and security. More information is available at www.keysight.com.
# # #
1 Gartner, Clouds Are Secure: Are You Using Them Securely? January 31, 2018
2 Gartner, Clouds Are Secure: Are You Using Them Securely? January 31, 2018
Additional information about Keysight Technologies is available in the newsroom at www.keysight.com/go/news, Keysight blog, and on Facebook, Google+, LinkedIn, Twitter and YouTube.
Contact:
Beth Hespe, Americas and EMEAI
+1 609-994-7442
beth.hespe@keysight.com
Fusako Dohi, Asia
+81 42 660-2162
fusako_dohi@keysight.com