SANTA ROSA, Calif., May. 31, 2018
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world, announced the first DDR51 and LPDDR52 Protocol Debug and Validation solutions. These solutions, when used in conjunction with Keysight's U4164A logic analyzer, enable designers of enterprise servers, mobile devices, and wireless equipment to debug and test DDR5 and LPDDR5 systems as well as validate protocol compliance.
Industry adoption of the 5G New Radio (NR) standard requires data servers and mobile devices to offer higher data rates and performance, as well as support lower power consumption. DDR5 Memory delivers higher bandwidth and performance improvements that the next generation of cloud servers need to support 5G use cases. LPDDR5 enables mobile devices to support increased bandwidth, improved performance, and lower power consumption.
New solutions from Keysight provide engineers with critical insight into the behavior of the DDR5 or LPDDR5 bus traffic by capturing and analyzing live traffic. This is achieved by tracing signals in the memory bus between the processor and memory devices.
Keysight provides comprehensive design test solutions for next generation cloud servers by combining its DDR5 Analysis and Compliance Validation software and U4164A logic analyzers with DDR5 interposers3.
"Critical cloud and device applications require reliable and high performing DDR5 memory technology. Keysight's DDR5 and LPDDR5 Memory Protocol Debug and Validation solutions enable device designers to accelerate high-speed digital interface innovations in support of next generation devices and future 5G use cases," said Kailash Narayanan, vice president and general manager for Wireless Device and Operators at Keysight.
Keysight offers a comprehensive portfolio of solutions to address the entire DDR5 technology lifecycle from design to debug, compliance validation, and manufacturing testing of mature products. Common user interfaces, combined with extensive test coverage across the workflow creates a cost-efficient test environment that offers the superior correlation of measurements necessary to resolve issues related to memory traffic, signal integrity and power integrity.
Additional information
Keysight's U4164A 4 Gb/s state logic analyzer is available at www.keysight.com/find/U4164A
FuturePlus system's FS2600 or FS2604 RDIMM/LRDIMM interposers is available at: www.futureplus.com
Keysight's Memory Analysis SW with performance and compliance test solutions for logic analysis is available at www.keysight.com/find/B4661A
Information on compatible probes made by Keysight channel partner FuturePlus is available at: www.keysight.com/find/FuturePlus
About Keysight in 5G
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $3.2B in fiscal year 2017. In April 2017, Keysight acquired Ixia, a leader in network test, visibility, and security. More information is available at www.keysight.com/find/5G.
1DDR5 – the fifth generation of Double Data Rate Synchronous Dynamic Random Access Memory
2LPDDR5 – Low Power DRAM technology, evolved to the fifth-generation(LPDDR5) to deliver significant reduction in power and extremely high bandwidth compared to LPDDR4
3DDR5 interposers are provided by Keysight's premier channel partner FuturePlus Systems
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers, and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor, and general electronics end markets. Keysight generated revenues of $3.2B in fiscal year 2017. In April 2017, Keysight acquired Ixia, a leader in network test, visibility, and security. More information is available at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at www.keysight.com/go/news and on Facebook, Google+, LinkedIn, Twitter and YouTube.
Contact:
Geri Lynne LaCombe, Americas
+1 303 662 4748
[email protected]
Magda Antone, Europe
+34 (93) 3434612
[email protected]
Connie Wong, Asia
+852 3197-7818
[email protected]