SANTA ROSA, Calif., October 15, 2019
Keysight Technologies, Inc. (NYSE: KEYS), a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world, announced an extended collaboration with Integrated Device Technologies, Inc. (IDT), a wholly owned subsidiary of Renesas Electronics Corporation (TSE: 6723), on component characterization of 5G new radio (NR) mmWave integrated circuit (IC) beamformers to accelerate development of 5G NR base stations.
Network equipment manufacturers (NEMs) use beamforming technology in 5G NR base stations to improve reliability and efficiency in the mmWave frequency spectrum. Beamforming uses multiple antennas (a phased array) to transmit the same signal, thereby increasing the signal strength to and from a chosen direction to extend cellular coverage, delivering higher data rates and an improved radio environment.
“Our close collaboration with Keysight enables us to validate that our 5G beamformers and other components deliver the high performance and low-power consumption essential for 5G network infrastructure equipment,” said Naveen Yanduru, vice president and general manager of IDT’s RF product division.
As the bandwidth of integrated circuits using 5G technology increases, it is important to characterize their performance over wider frequency ranges. This is why IDT uses Keysight’s high performance family of vector network analyzers (VNAs) to validate the performance of its beamformer ICs. Keysight solutions enable IDT, and other leading designers of ICs, to measure key parameters such as scattering (S) parameters, 1dB compression point (P1dB), third-order intermodulation products (IM3), and error vector magnitude (EVM).
“Our extended collaboration with IDT demonstrates how Keysight’s 5G beamformer IC test solutions enable designers of beamformers to validate performance using high precision measurement and simulation tools, ensuring reliable and efficient designs,” said Kailash Narayanan, vice president and general manager of Keysight's wireless test group.
The two companies will use the Keysight Streamline USB VNA to demonstrate IDT’s active beamforming radio frequency integrated circuit (RFIC) for 5G NR at the 2019 IEEE International Symposium on Phased Array Systems and Technology (Array2019) taking place October 15 – 18, 2019 in Waltham, MA.
Earlier this year, at the world’s largest microwave and RF industry trade show – the International Microwave Symposium (IMS) 2019 – IDT showcased a 64-element phased array antenna comprised of its 5G NR beamformer ICs and wideband microwave synthesizer. The demonstration leveraged Keysight’s Signal Studio software for signal creation, the PXI vector signal generator for waveform generation and the UXA Signal Analyzer for vector signal analysis, enabling them to validate the signal fidelity performance of its beamforming IC.
About Keysight in 5G
Keysight’s industry-first 5G end-to-end design and test solutions enable the mobile industry to accelerate 5G product design development from the physical layer to the application layer and across the entire workflow from simulation, design, and verification to manufacturing, deployment, and optimization. Keysight offers common software and hardware platforms compliant to the latest 3GPP standards, enabling the ecosystem to quickly and accurately validate 5G chipsets, devices, base stations and networks, as well as emulate subscriber behavior scenarios. Additional information about Keysight's 5G solutions is available at www.keysight.com/find/5G.
About Keysight Technologies
Keysight Technologies, Inc. (NYSE: KEYS) is a leading technology company that helps enterprises, service providers and governments accelerate innovation to connect and secure the world. Keysight's solutions optimize networks and bring electronic products to market faster and at a lower cost with offerings from design simulation, to prototype validation, to manufacturing test, to optimization in networks and cloud environments. Customers span the worldwide communications ecosystem, aerospace and defense, automotive, energy, semiconductor and general electronics end markets. Keysight generated revenues of $3.9B in fiscal year 2018. More information is available at www.keysight.com.
# # #
Additional information about Keysight Technologies is available in the newsroom at https://www.keysight.com/go/news and on Facebook, LinkedIn, Twitter and YouTube.
Keysight Contact:
Geri Lynne LaCombe, Americas/Europe
+1 303 662 4748
geri_lacombe@keysight.com
Fusako Dohi, Asia
+81 42 660-2162
fusako_dohi@keysight.com